Pressure Calculator & Conversion Chart

Convert millibars to kilopascals and vice versa by using element14's pressure calculator below.
Our mass conversion chart also provides you with the multiplier for these conversions so you can make them manually when necessary.

Pressure Conversion Calculator

Pressure Conversion Chart

StartingMultiplierEnding
Atmosphere (atm)760Torr (Torr)
Atmosphere (atm)1.01325 Bar (b)
Atmosphere (atm)101.325Kilopascal (kPa)
Atmosphere (atm)101325Pascal (Pa)
Atmosphere (atm)1.0332274528Kilogram per Square Centimetre (kgf/cm2)
Atmosphere (atm)14.69596432068Pounds per Square Inch (psi)
Torr (Torr)0.001315789473684 Atmosphere (atm)
Torr (Torr)0.001333223684211 Bar (b)
Torr (Torr)0.1333223684211 Kilopascal (kPa)
Torr (Torr)133.3223684211 Pascal (Pa)
Torr (Torr)0.001359509806316 Kilogram per Square Centimetre (kgf/cm2)
Torr (Torr)0.01933679515879 Pounds per Square Inch (psi)
Bar (b)0.986923266716 Atmosphere (atm)
Bar (b)750.0616827042 Torr (Torr)
Bar (b)100 Kilopascal (kPa)
Bar (b)100000 Pascal (Pa)
Bar (b)1.019716212978 Kilogram per Square Centimetre (kgf/cm2)
Bar (b)14.50378911491 Pounds per Square Inch (psi)
Kilopascal (kPa)0.00986923266716 Atmosphere (atm)
Kilopascal (kPa)7.500616827042 Torr (Torr)
Kilopascal (kPa)0.01 Bar (b)
Kilopascal (kPa)1000 Pascal (Pa)
Kilopascal (kPa)0.01019716212978 Kilogram per Square Centimetre (kgf/cm2)
Kilopascal (kPa)0.1450378911491 Pounds per Square Inch (psi)
Pascal (Pa)0.00000986923266716 Atmosphere (atm)
Pascal (Pa)0.007500616827042 Torr (Torr)
Pascal (Pa)0.00001 Bar (b)
Pascal (Pa)0.001 Kilopascal (kPa)
Pascal (Pa)0.00001019716212978 Kilogram per Square Centimetre (kgf/cm2)
Pascal (Pa)0.0001450378911491 Pounds per Square Inch (psi)
Kilogram per Square Centimetre (kgf/cm2)0.9678411053541Atmosphere (atm)
Kilogram per Square Centimetre (kgf/cm2)735.5592400691 Torr (Torr)
Kilogram per Square Centimetre (kgf/cm2)0.980665 Bar (b)
Kilogram per Square Centimetre (kgf/cm2)98.0665Kilopascal (kPa)
Kilogram per Square Centimetre (kgf/cm2)98066.5 Pascal (Pa)
Kilogram per Square Centimetre (kgf/cm2)14.22335835237 Pounds per Square Inch (psi)
Pounds per Square Inch (psi)0.0680458919319 Atmosphere (atm)
Pounds per Square Inch (psi)51.71487786825 Torr (Torr)
Pounds per Square Inch (psi)0.0689475 Bar (b)
Pounds per Square Inch (psi)6.89475 Kilopascal (kPa)
Pounds per Square Inch (psi)6894.75 Pascal (Pa)
Pounds per Square Inch (psi)0.0703068835943 Kilogram per Square Centimetre (kgf/cm2)